Create a custom event
    Add a custom or change event by adding an external event to an object. 
External events allow you to manage object events.
- FromProject view, select the object that you want to contain the external event.
 - InPropertiesnext toEvents, select
Add external event. - Select the event to manage the events of another object.
 - ChooseSelect.The new event appears underEvents.
 - To link a method to the event, next to the event, select
Add new methodand then select the method. - ChooseSelect.
 - (optional) If the method requires arguments, expand the method and set the arguments.
 
Provide Feedback