Change objects order
    Move selected objects in front of or behind other objects in the editor.
- InProject view, double-click a container or select.
The editor opens a separate tab. - Select the object to move.TIP: To select multiple objects, holdCtrland select multiple objects.
 - In the editor toolbar, select the button to move the object in relation to other objects:
 Send to back. Send the object behind all objects in the editor.
 Send backward. Send the object behind the next object in the editor.
 Bring forward. Send the object in front of the next object in the editor.
 Bring to front. Send the object in front of all objects in the editor.
 
Provide Feedback