Create a library folder
    Create a folder in a local or remote library to organize the templates that belong to that library.
- From the main toolbar, select.Template Libraries
 - Select a library in which you want to add a folder.
 - InTemplate Libraries, selectand select
New folder. - (optional) Enter a name for the folder.
 
New folder appears under the selected library in 
Template Libraries
.Provide Feedback