Network interfaces variables
    Bind a property of graphic object to a predefined 
Network interfaces 
variable in the Additional IP addresses 
object to configure the network for your HMI device. For example, bind to the IP addresses 
variable to specify the IP address for the HMI device. To bind to a variable, see Create dynamic links.The 
    
Additional IP addresses
 category under Network interfaces
 in the Dynamic Link browser displays the variables related to the HMI device.
        
  Variable  | Type  | Definition  | Read or Write  | Reboot Required  | 
|---|---|---|---|---|
Interface name  | String  | Name of the interface  | Read-only  | Reboot not required  | 
DHCP activated  | Boolean  | Obtain IP settings automatically using DHCP  | Read/Write  | Reboot required  | 
IP address  | String  | IP address of the network  | Read/Write  | Reboot required  | 
Mask  | String  | Subnet mask of the network  | Read/Write  | Reboot required  | 
DNS 1  | String  | Primary DNS address of the network  | Read/Write  | Reboot required  | 
DNS 2  | String  | Secondary DNS address of the network  | Read/Write  | Reboot required  | 
Default gateway  | String  | IP address of the default network gateway  | Read/Write  | Reboot required  | 
Provide Feedback