Position

Alignment of the control to the container
BrowseName
Position

Values

Value
DisplayName
Description
0
Top left
Element is docked to the top left corner
1
Top center
Element is docked to the center of the top border
2
Top right
Element is docked to the top right corner
3
Left center
Element is docked to the center of the left border
4
Center
Element is centered (vertically and horizontally) to the container
5
Right center
Element is docked to the center of the right border
6
Bottom left
Element is docked to the bottom left corner
7
Bottom center
Element is docked to the center of the bottom border
8
Bottom right
Element is docked to the bottom right corner
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal