FactoryTalk Optix Application
    You develop and compile 
FactoryTalk Optix Applications
 in FactoryTalk Optix Studio
. The compiled applications can be deployed to Windows®
 or Linux client systems.Application structure
      Each compiled 
FactoryTalk Optix Application
 contains these files and folders:
        - Executable file that starts the application:(Windows)FTOptixRuntime.exefile.(Linux)FTOptixRuntimefile.
 - Bindings,Core, andModulesfolders. Contain runtime binary files.
 - Application runtime logs:(Windows)Logfolder.(Linux)folder./persistent/log/Rockwell_Automation/FactoryTalk_Optix
 - Projectsfolder. Contains a folder for each compiled project (application). Each project folder contains:
- ApplicationFilesfolder. Contains files generated at runtime, such as embedded databases, databases for retentivity functions, and temporary files.
 - ProjectFilesfolder. Contains all files in use in the project, including images, fonts, documents, and these subfolders:
- NetSolutionfolder. Contains the .NET assemblies obtained from C# NetLogics.
 - PKIfolder. Contains private, public, and refused certificates for OPC UA authentication.
 
 - .optixproject file.
 
 - Auxiliary files, including theFTOptixRuntime.xmlconfiguration file.
 
Provide Feedback