Start debugging on the remote machine
    Deploy the runtime application to the remote machine and start the debugging process on the development machine.
Prerequisites
- To start debugging on the remote machine
 - From the main toolbar, select
 Open .NET Solution.The default external code editor opens.TIP: Rockwell Automation recommends using Microsoft Visual Studio 2022 or Microsoft Visual Studio Code as the default code editor. Some development assistance features may not be available when using a different code editor. - FromFactoryTalk Optix Studio, deploy theFTOptixApplicationto the target device.For more information, see Deploy a FactoryTalk Optix Application.
 - In Visual Studio, configure and start the debugging process.Attach to process with these settings:
- ConnectionType
 - Default.
 - ConnectionTarget
 - The name and port that you obtained while performing Prepare the remote machine for debugging.
 - Available Process
 - FTOptixRuntime.exe
 
 
Provide Feedback