Communication drivers overview
    Some communication drivers may have specific characteristics.
     IMPORTANT: 
    For the TwinCAT driver, FactoryTalk Optix cannot import tags of the ITCommObjectServer type because the ITCommObjectServer type is not exported into the TwinCat tpy file.
Communication driver  | Online tags import  | Offline tags import  | 
|---|---|---|
MELSEC Q driver  | ||
CODESYS Driver  | ||
TwinCAT driver  | ||
Serial port  | ||
Provide Feedback