Open the project in an external code editor
    You can open the entire project in an external code editor.
Prerequisites
Set the default external code editor. See Set the default code editor.
- To open the project in an external code editor
 - From the main toolbar, select
 Open .NET Solution.The default external code editor opens.TIP: Rockwell Automation recommends using Microsoft Visual Studio 2022 or Microsoft Visual Studio Code as the default code editor. Some development assistance features may not be available when using a different code editor. 
Provide Feedback