Configure a widget to display logged alarms
    Add a widget that displays historical data about alarms at runtime.
- From the toolbar, select.Template Libraries
 - InLibraries, search forAlarm History Grid with filter.
 - UnderComponents, dragAlarm History Grid with filterontoPage3 (type)inProject view.
 - SelectClose.
 - InProject view, selectFilteredAlarmHistoryGrid1.
 - InProperties, setHorizontal alignmenttoStretch.The object adjusts its width to the container at runtime.
 - Create a dynamic link betweenAlarmsEventLoggerand .For more information about dynamic links, see Create dynamic links.
 
Filtered Alarms History Grid with filter in Page3

Provide Feedback