LogicObject.GetAlias(string)
    Returns an 
IUANode
 C# object that corresponds to the node pointed to by the alias passed in the argument. Access the node to which a known alias pointsstatic IUANode GetAlias(stringaliasName);
Arguments
      - aliasName(string)
 - TheBrowseNameof the alias.
 
Returns
      - IUANode
 - A C# object that corresponds to the node pointed to by the alias.
 
Example
      The following example shows an API that returns a C# object corresponding to the node pointed to by the alias 
Motor
, which Speed
 property value is read and assigned to the myMotorSpeed
 variable.
     TIP: 
    The 
(MotorType)
 cast operator changes the object type returned by the API from IUANode
 to MotorType
. This is useful if you want to access the Speed
 property of refMotor
 directly.var refMotor = (MotorType)LogicObject.GetAlias("Motor"); var myMotorSpeed = refMotor.Speed;
Provide Feedback