Commit changes to a local repository
    Save changes to a project to save changes on the local computer only. Saved changes are not backed up to a repository. Commit changes so that the changes are backed up to the local repository that is in the project folder on the local computer.
- Select.
 Save and Commit - If version control is not configured and the message "You must configure a User Name and Email in FactoryTalk Studio Options before making a commit" appears:
- In the title bar ofFactoryTalk Optix Studio, select.
 FactoryTalk Optix Studio Options - SelectVersion control.
 - UnderVersion Control User Configuration, inUser Name, type your username.TIP:User Nameis the name that appears next to commits when you openView historyfor a project. View history identifies your commits with the first letter of your user name.
 - InUser Email, type your email address.
 - SelectSave.
 
 - InSave and commit, inCommit message, type a description of the changes you are committing.
 - SelectOK.
 
Provide Feedback