Create a local project
    Create a local project with version control to create the local project and a local repository on your computer. The local repository allows you to commit changes to your project and provides version control to view and restore previous versions of your project.
- If there is an openFactoryTalk Optixproject, selectand then select
 ProjectClose Project. - SelectCloseor if there are changes to save, selectSave and close.
 - On the Start page, selectNew.
 - Select the type of project.
 - InName, enter the name of the project.TIP: The project and repository names must be the same, including capitalization.
 - InLocation, type the path to the project.
 - SelectUse version control.TIP: When version control is enabled for a local project and you want to back up the project to a remote repository, push the local changes to associate the local project with a remote repository.
 - SelectCreate.
 
Version control is added to the new project.
Provide Feedback