Configure an application as an MQTT client
    Message Queue Telemetry Transport (MQTT) is a standard ISO protocol based on a message broker, which is responsible for distributing messages to recipient clients.
Application example

     TIP: 
    
You can download a sample project from:
 MQTTClient.zipPrerequisites
- Add the NuGet Gallery | MqttNet third-party library. See Third-party .NET libraries.
 
- To develop the project
 - Save the project.
 
Select 
  to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.
Run
Provide Feedback