Duplicate a data logger
    Duplicating a data logger configures a new logger based on the existing logger.
- From the toolbar, select.Open dashboard page
 - In the central pane, selectConfigure a data logger.
 - Right-click the data logger to duplicate and selectDuplicate.A new data logger appears in the list of available data loggers.
 
Edit the duplicated logger settings. See Edit a data logger.
Provide Feedback