Edit a data logger
    Edit an existing data logger.
Prerequisites
Either:
        
- To edit a data logger
 - From the toolbar, select.Open dashboard page
 - In the central pane, selectConfigure a data logger.
 - Select the data logger to edit.
 - If needed, edit the loggerNameand properties.
 - SelectNext.
 - If there is no database for the logger, create a database:TIP: You can also right-click an existing database and selectDuplicate. Duplicating a database is useful if you want to create a database based on an existing database.
- SelectNew databaseand complete:
- Name. A name for the database.
 - Type. EitherEmbeddedorODBC connection.
 
 - SelectNext.
 - Set the database properties.
 - SelectNext.
 
 - Select the database to store the logger data and selectNext.
 - Select the variables that you want to log and selectNext.TIP: You can find variables by using the search field.
 - SelectExit.
 
- (optional) Set a deadband interval.
 - (optional) Store read operation codes.
 - (optional) Store variable reading date and time.
 
Provide Feedback