Duplicate a graphic object
    Copy and paste an object to duplicate the configuration of the object. Duplicated objects create consistency and save time when creating objects.
- InProject viewor in the editor, right-click the object to duplicate and selectCopy.TIP: You can also select the object and press .
 - InProject viewor in the editor, right-click the object to contain the duplicated object and selectPaste.TIP: You can also select the object to contain the duplicated object and press .
 
Provide Feedback