Configure a switch to simulate alarms
    Configure a switch that simulates Motor1 alarms.
- InProject view, double-clickPage2 (type).
 - Right-clickPage2 (type)and select .
 - InProperties, create a dynamic link betweenCheckedand theMotor1Alarmvariable.For more information about dynamic links, see Create dynamic links.
 - In the editor, arrangeSwitch1according to your preferences.
 
Switch to simulate alarms at the bottom of Page2

At runtime:
        
- Toggle the switch to trigger an alarm.
 
Provide Feedback