Configure an alarm grid
    Add a table that displays alarms status in real time.
- From the toolbar, select.Template Libraries
 - InLibraries, search forAlarm Grid.
 - UnderComponents, dragAlarm GridontoPage2 (type)inProject view.AlarmGrid1appears underPage2 (type).
 - SelectClose.
 - InProject view, selectAlarmGrid1.
 - InProperties, setHorizontal alignmenttoStretch.The object adjusts its width to the container at runtime.
 
AlarmGrid1 in Page2

Provide Feedback