Commit a library
    Commit changes to a local or remote library to save changes on the local computer only. Committed changes are not backed up (or pushed) to a remote repository.
Prerequisites
- To commit a library
 - From the main toolbar, select.Template Libraries
 - Select
 Commit. - Enter a meaningful commit message.
 - SelectOK.
 
A new version of the library is saved on the local computer.
Provide Feedback