Configure a remote library
    Configure a remote library to store templates of objects and variables on a remote Git repository.
Prerequisites
Obtain the URL of the remote Git repository to store the library and user credentials.
        
    
    
     IMPORTANT: 
    Verify that the Git repository is safe to store the remote library. Contact a repository administrator to learn who can access the repository.
- To configure a remote library
 - From the main toolbar, select.Template Libraries
 - InTemplate Libraries, selectand select
New remote library. - InRemote location, enter the URL to the Git repository to store the library.
 - (optional) Enter a name for the library.
 
New remote library appears in 
Template Libraries
.- Add templates to your library. See Create a template.
 
Provide Feedback