Create a template
    Use a template to create objects, object types, and variables that have similar attributes.
- Select.Template Libraries
 - FromProject view, drag the node into a library inTemplate Libraries.For example, drag an object, object type, variable, or widget.A new template appears underComponents.
 - (optional) Select the template and enter a description.For example, explain how to use or implement the object, object type, variable, or widget.
 
Provide Feedback