Create a linear gauge
    Create a linear gauge that shows the temperature.
- InProperties, right-clickMainWindow (type)and select .
 - InProperties, set theEditablevariable value toFalse.
 - Create a variable:
- InProperties, at the top, selectand select
Analog variable. - Create a complex dynamic link between theAnalogVariable1property and the actualAnalogVariable1variable by using binding mode.
              - DynamicLink
 - EU Mode
 - Localize.
 
 - Create a dynamic link betweenLow limitand
 - Create a dynamic link betweenHigh limitand
 - SetConstraintoTrue.
 
For more information about dynamic links, see Create dynamic links. - Link the variable alias:
- InProperties, create a dynamic link betweenValueand .
 - Create a dynamic link betweenMinimum valueand .
 - Create a dynamic link betweenMaximum valueand .
 
For more information about dynamic links, see Create dynamic links. 
Provide Feedback