Session nodes
    The 
{Session}
 alias points to the Session
 node for the current runtime session. FactoryTalk Optix Studio
 automatically creates dynamic links with the nodes inside of the Session
 node.Session nodes include:
        
  
    
Node  | Description  | 
|---|---|
Groups  | Groups can be defined and used the project. Each group displays a value:
                     
  | 
MeasurementUnits  | List of the available amounts. Each amount has properties based on the locale:
                     
  | 
Locale  | Array of session locale IDs. This node specifies all of the locales supported by the user interface.  | 
User  | Properties for the user:
                     
  | 
Provide Feedback