Conditional converter
    Verify if the source variable value is 
True
 or False
.Properties
      
  Property  | Description  | 
|---|---|
True value  | The value of the expression that is  True . | 
False value  | The value of the expression that is  False . | 
Mode  | The direction of the dynamic link:
         
  | 
Source
      The condition variable (Boolean).
Output
      A 
True
 or False
 value.Example
      In the following example, the conditional converter:
        
- Sets the text color of a label to green if a switch is selected.
 - Sets the text color of a label to red if a switch is cleared.
 

Provide Feedback
Read from the source node to the parent.
Write from the parent to the source node.
Read from the source node to the parent and write from the parent to the source node.