Configure security for content at runtime
    Configure the security of a screen or content at runtime for users in a group or role. For example, specify whether a screen or content is Visible or Enabled by creating a dynamic link from those properties to a group or role Session variable. 
Create users and groups or roles and then assign users to groups or roles.
- InProject view, select the screen or graphic object.
 - InPropertieshover over the property and then select.
 Add Dynamic Link - In the dynamic link browser, expandAliases > Session > Session.
 - Set the value of the property for a:
- Group. ExpandGroupsand select the group.
 - Role. ExpandRolesand select the role.
 
TIP: To set the same property value for additional groups and roles, in the property, create a complex dynamic link with an expression evaluator or other necessary logic. See Create a complex dynamic link. 
Provide Feedback