Add a locale language to a localization dictionary
    Add locale languages to a localization dictionary so you can change the language displayed for an application at runtime.
- InProject view, expandTranslationsand double-click a localization dictionary.
 - In the localization dictionary, in theTranslation tableview, selectAdd locale.
 - UnderSelect the new locale, select a locale language and then select.

 - InNew locales added, to add the locale to the displayed objects, selectYes.
 
A new column appears for the locale.
Provide Feedback