Configure an alarm event logger
    Store logs about past events related to alarms in a database.
- InProject view, right-clickDataStoresand select .
 - Hover-overEmbeddedDatabase1, select, and enter
AlarmDB. - From the toolbar, select.Template Libraries
 - InLibraries, search forAlarms Event Logger.
 - UnderComponents, dragAlarms Event LoggerontoLoggersinProject view.
 - SelectClose.
 - InProject view, selectAlarmsEventLogger1.
 - InProperties, create a dynamic link betweenDatabaseand .For more information about dynamic links, see Create dynamic links.
 
Provide Feedback