Paths
    You can use path shortcuts when developing your application logic.
Shortcut  | Description  | 
|---|---|
%PROJECTDIR%  | A directory that contains files transferred at runtime (images, documents, and so on). Example:  C:\Users\ UserName \Documents\Rockwell Automation\FactoryTalk Optix\ ProjectName  | 
%APPLICATIONDIR%  | A directory that contains objects used at runtime, including these objects:
                   
  | 
%USB ,N %where  N  is a number associated with the USB device. | A path to a specific USB device connected to the target device.  | 
Provide Feedback