Make an active alarm visible
    Configure the 
Active
 property of a graphic object to make an alarm visible at runtime. Dynamically link the Active
 variable of the graphic object to the Active
 variable of an alarm. At runtime, the appearance of the graphic element changes when the alarm is active. The 
Active
 variable requires no scripting or NetLogic. For example, you can create a digital alarm and then bind the Active
 property of a graphic element, such as an LED, to the Active
 variable of a digital or other alarm. The LED lights up at runtime when the alarm reaches its configured limits or state.Prerequisites
- Add an LED graphic object to a window
 - Create and configure an alarm
 
- To make an active alarm visible
 - FromProject view, open the window that contains the LED and select the LED.
 - InPropertiesfor the LED, inActive, select.
 Change Dynamic Link - In theDynamic Link Editor, expand theAlarmsfolder and expand the alarm.
 - Select theActivevariable for the alarm.In the case of Exclusive and Non-Exclusive alarm types, you can create a dynamic link to a specific alarm state (high-high, high, low, or low-low).
 - ChooseSelect.
 
The LED will now light with the color indicated in 
Properties
 when the alarm is active. The default color for the LED is red.Provide Feedback