Add a third-party library to the Visual Studio project
    Add a third-party .NET library.
Prerequisites
Set Visual Studio as the default external code editor. See Set the default code editor.
- To Add a third-party library to the Visual Studio project
 - Copy the .NET assembly for the library to theProjectFiles/NetSolutionproject folder.
 - From the main toolbar, select
 Open .NET Solution.The default external code editor opens.TIP: Rockwell Automation recommends using Microsoft Visual Studio 2022 or Microsoft Visual Studio Code as the default code editor. Some development assistance features may not be available when using a different code editor. - Update the reference by selecting the assembly from 1.For more information, see Manage references in a project - Visual Studio (Windows) | Microsoft Learn.
 
Provide Feedback