ResourceURI.FromApplicationRelativePath(path)
    Returns a C # object of the 
ResourceURI
 type, with the URIType
 of ApplicationRelative
 that contains a relative path to a file in relation to the ApplicationFiles
 folder.static ResourceUri FromApplicationRelativePath(stringpath);
Arguments
      - path(string)
 - A relative path to a file in relation to theApplicationFilesfolder.
 
Returns
      - ResourceURI
 - A C# object that contains the path indicated in the argument.
 
Example
      The following example shows an API that returns a C# 
applicationRelativeResourceURI
 object of the ResourceURI
 type that contains the Text1.txt
 relative path. The object is used as an argument of the .NET WriteAllText API
 to create a Text1.txt
 text file inside theApplicationFiles
folder.
        var applicationRelativeResourceUri = ResourceUri.FromApplicationRelativePath("Text1.txt"); Log.Info(applicationRelativeResourceUri.ApplicationRelativePath); File.WriteAllText(applicationRelativeResourceUri.Uri, "Hello world!");
Provide Feedback