IUANode.Add(child)
    Adds a project node that corresponds to the C# object passed in the argument.
void Add(IUANodechild);
Arguments
      - child(IUANode)
 - A C# object that corresponds to the project node to add.
 
Example
      The following example shows that the 
MyLabel
 label child of the Panel
 object is added in the project:
        var newPanel = InformationModel.MakeObject<Panel>("Panel"); var newLabel = InformationModel.MakeObject<Label>("MyLabel"); newPanel.Add(newLabel);
Provide Feedback