Application variables
    Bind the property of a graphic object to a predefined 
Application
 variable to configure the FTOptixApplication
. For example, bind to the visibility of a property to make the object blink based on a machine or process state.To bind to a variable, see Create dynamic links.The 
Application
 category in the Dynamic Link browser displays the variables related to the FTOptixApplication
.Variable  | Type  | Definition  | Read or Write  | Reboot Required  | 
|---|---|---|---|---|
Blink fast  | Boolean  | Variable value that alternates between set for 1 second and cleared for 0.5 seconds.  | Read-only  | Reboot not required  | 
Blink medium  | Boolean  | Variable value that alternates between set for 2 seconds and cleared for 1 second.   | Read-only  | Reboot not required  | 
Blink slow  | Boolean  | Variable value that alternates between set for 3 seconds and cleared for 1.5 seconds.  | Read-only  | Reboot not required  | 
Provide Feedback