Add a Station Connection Status widget
    Add a Station Connection Status widget to monitor the controller connection status.
Prerequisites
- To add a Station Connection Status widget
 - From the main toolbar, select.Template Libraries
 - InLibraries, search forStation Connection Status.
 - UnderComponents, dragStation Connection StatustoMainWindow (type)or a different UI container inProject view.
 - InProperties, create a dynamic link betweenStationand the communication driver station that you want to monitor.For more information about dynamic links, see Create dynamic links.
 
At runtime, the widget displays these LED status indicators:
        
- Green LED. Connected to the controller.
 - Red LED. Disconnected from the controller.
 
Provide Feedback