Configure a communication driver
    Configure a communication driver to import tags in the online or offline mode.
Prerequisites
- Learn about any specific considerations for your controller. See Communication drivers overview.
 - If you import tags in the offline mode, export tags from a supported controller to a file. See the controller user assistance.
 
- To configure a communication driver
 - From the toolbar, select.Open dashboard page
 - SelectConfigure communications to devices.
 - SelectNew station.
 - Select a station type.
 - (optional) Edit the name of the station.
 - SelectNext.
 - Fill in the properties and selectNext.
 - SelectNext.
 - Configure tags import for the station:TIP: Some communication drivers may not support importing tags from controllers in the online mode, offline mode, or both modes.
- To import tags in the online mode, set the toggle toOnline.
 - To import tags in the offline mode, set the toggle toOfflineand inFile path, provide a path to the file with exported controller tags.
 
TIP: To select the station object inProject view, selectSelect in property view. - Select the tags of interest and selectNext.
 - (optional) To configure another communication driver, selectConfigure another deviceand repeat the procedure.
 - SelectExit.
 
In 
Project view
, the variables corresponding to the selected tags are added.If you imported tag types, create instances from the imported tag types. See Create an instance of a tag type.
Provide Feedback