HTTP methods
    The REST API Client NetLogic exposes these HTTP methods: GET, POST, PUT.
Get
      Use the GET method to request data from an API endpoint.
        
  
    
Argument  | Description  | 
|---|---|
apiUrl  | Address of an endpoint to access the API.  | 
queryString  | Arguments to pass to the API endpoint.  | 
bearerToken  | Token to authenticate the request.  | 
Post
      Use the POST method to send data to an API endpoint and create a resource on the server.
        
  
    
Argument  | Description  | 
|---|---|
apiUrl  | Address of an endpoint to access the API.  | 
requestBody  | Data to send to the server behind the API endpoint.  | 
bearerToken  | Token to authenticate the request.  | 
contentType  | The original media type of the resource.  | 
Put
      Use the PUT method to send data to an API endpoint and create or replace a resource on the server.
        
  
    
Argument  | Description  | 
|---|---|
apiUrl  | Address of an endpoint to access the API.  | 
requestBody  | Data to send to the server behind the API endpoint.  | 
bearerToken  | Token to authenticate the request.  | 
contentType  | The original media type of the resource.  | 
Provide Feedback