Manage translations
    Use C# APIs to read or write the translated strings inside the 
LocalizationDictionary
 objects.The APIs are supplied by the 
InformationModel
 static class.LocalizedText class
      LocalizedText
 classEvery API has an instance of the 
LocalizedText
 C# class among its own arguments, which identifies a key/line or specific string translated in a LocalizationDictionary
. It contains the following properties:
        - NamespaceIndex(int)
 - Identifier of the namespace of the project to which theLocalizationDictionarybelongs.TIP: If theLocalizationDictionaryis in the same NetLogic project, you do not need to specify theNamespaceIndexin the construction of aLocalizedText.
 - TextId(string)
 - A key with which the translations of a string can be associated.
 - LocaleId(string)
 - A locale ID. For example:en-US.
 - Text(string)
 - A translated string.
 
Provide Feedback