Set dynamic variables polling time for alarms
    Set the time interval between readings of variable values from OPC UA servers and tag values from controllers.
- InProject view, select the root project node.
 - InProperties, setDynamic variables polling time.TIP: Set the polling time between one sampling and the next in HHHH:MM:SS.MS format.
 
Provide Feedback