Recipes editor
    The recipes editor widget contains the graphical objects and NetLogics required to display and manage the recipes at runtime.
Use the recipes editor widget to:
      
- Display ingredients and values of a stored recipe during editing or loading the controller
 - Create, edit, or delete a recipe
 - Store a recipe in the database
 - Load a recipe from theFactoryTalk Optix Applicationto the controller
 - Load a recipe from the controller to theFactoryTalk Optix Application
 
Interface
      Recipes editor interface

Item  | Name  | Description  | 
|---|---|---|
![]()  | Recipe name  | Assign a name to a new recipe or select an existing recipe.  | 
![]()  | Recipe control buttons  | 
  | 
![]()  | Ingredients list  | Recipe schema ingredients.  | 
![]()  | Ingredient values editor  | Editable values of the recipe ingredients.  | 
![]()  | Applied ingredient values  | Values of the ingredients on the controller.  | 
Provide Feedback