Configure a recipe
    Create a recipe schema that uses the Ingredient01, Ingredient02, and Ingredient03 variables.
- From the toolbar, select.Open dashboard page
 - In the central pane, selectConfigure a recipe.
 - SelectNew recipe.
 - Create a dynamic link betweenTarget nodeand:
- If you created variables, .
 - If you imported Logix controller variables, .
 
 - SelectNextand selectNext.
 - SelectNew database.
 - InName, enterRecipeDBand selectNext.
 - SelectNextand selectNext.
 - SelectIngredient01,Ingredient02, andIngredient03, and selectNext.Selected variables

 - SelectExit.
 
In 
Project view
, RecipeSchema1
 appears under Recipes
.Provide Feedback