References to dynamic link sources
    Depending on the type of a dynamic link source, the property value field displays the reference in different ways.
Property values
      
  Source type  | Property value  | 
|---|---|
A node or a variable  | The  BrowseName  of the source. | 
An attribute of a node or of a variable  | BrowseName@ name of the attribute  | 
An array variable  | BrowseName[ array index values ] | 
An array index of the array variable  | BrowseName[ array index number ]For example,  [0]  is the first array index. | 
A bit index   | BrowseName[ bit index number ]
                
                For example, [0] is the first bit index.  | 
A property of a node  | The path to the source node.  | 
A node or a variable formatted by the user  | The information about the source followed by  (formatted)  | 
Reference type  | Description  | Property value example  | 
|---|---|---|
Absolute  | A complete path to the referenced source that starts with the root directory.  | ProjectName/Model/SourceVariable  | 
Relative  | A path to the referenced source that starts with the target node directory.  | ../SourceVariable  | 
With aliases  | Any type of a path that contains aliases. An alias is a variable type that points to a source node and has a unique identifier property. For more information, see Aliases.  | {Motor}/Speed  | 
     TIP: 
    
Selecting the blue link (
../SourceVariable
 in the example), brings you to the link target (SourceVariable
 node).
Provide Feedback