Manage client devices
    Add, remove, duplicate, and select target client devices available in the network.
The default target client device, the 
Emulator
, runs locally on the development computer. The Emulator
 is useful for testing FactoryTalk Optix Applications
 and does not require you to install the FactoryTalk Optix Application Update Service
 software. 
     TIP: 
    Rebooting the 
Emulator
 is not supported so that you do not accidentally reboot a device on which Windows®
 is installed. Provide Feedback