Configure a transitioned event
    Trigger methods if the value of a variable or object property meets a specific condition.
- InProject view, select an object or a variable.
 - InProperties, right-click a variable or a property and select .TIP: If needed, selectto add a variable.

 - InEvents, fromTransitionselect:
- Equal to
 - Not equal to
 - Greater than
 - Greater than or equal to
 - Less than
 - Less than or equal to
 
 - Set theValueproperty.TIP: You can enter the threshold value or add a dynamic link to the threshold value. For more information about dynamic links, see Create dynamic links.
 - Next toVariableTransitioned, select.

 - Select a method:
- For global methods, expandCommands.
 - For local methods, expand the nodes that expose methods (for example, aDataGridnode exposes aRefreshmethod), or expand the node related to a specific NetLogic.
 
 - (optional) If the method requires arguments, expand the method and set arguments.
 
Provide Feedback