ResourceURI.FromProjectRelativePath(path)
    Returns a C# object of the 
ResourceURI
 type, with the URIType
 of ProjectRelative
 and that contains a relative path to a file than the ProjectFiles
 folder.static ResourceUri FromProjectRelativePath(stringpath);
Arguments
      - path(string)
 - A relative path of a file in relation to theProjectFilesfolder.
 
Returns
      - ResourceURI
 - A C# object that contains the path indicated in the argument.
 
Example
      The following example shows an API that returns a C# 
projectRelativeResourceURI
 object of the ResourceURI
 type that contains the relative path Text1.txt
. The object is used as an argument of the .NET WriteAllText
 API to create a Text1.txt
 text file inside the ProjectFiles
 folder.
        var projectRelativeResourceUri = ResourceUri.FromProjectRelativePath("Text1.txt"); Log.Info(projectRelativeResourceUri.ProjectRelativePath); File.WriteAllText(projectRelativeResourceUri.Uri, "Hello world!");
Provide Feedback