Develop automatically generated UI
    Develop a UI populated automatically with graphical elements based on the properties of objects in the Model folder.
     NOTE: 
    
Download a sample project:
 UIGeneratedFromModel.zipExample application


Prerequisites
- Download, extract, and copy the images into thefolder.ProjectName/ProjectFiles
 
- To develop the project
 - Arrange the interface elements.
 - Save the project.
 

Select 
  to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.
Run
Provide Feedback