Export translated strings to a CSV file
    Export strings to use in the strings another project and help prevent having to recreate and translate the strings. Export translated strings to a CSV file using the predefined script in the template library. 
- In the main toolbar, select.Template Libraries
 - SelectScripts.
 - UnderComponents, dragTranslations Importer and Exporterinto the project node orTranslationsfolder.
 - InTemplate Libraries, selectClose.
 - WithImport and Export Translationsselected, inProperties, inCSVPath,browse to select the .CSV file.
 - InCharacterSeperator, select the separator.
 - InProject view,right-clickImport and Export Translationsand then selectExecute ExportTranslations.
 
Provide Feedback