Push Agent
    The Push Agent script sends data from a data logger to the cloud.
Operation
      Push Agent periodically acquires data from a data logger and sends the data to the cloud in the 
JSON
 format. Push Agent implements the store and forward mechanism that acquires data from a data logger and saves the data in an auxiliary store from which the data is extracted and sent to the cloud.Transfer modes
      Push Agent supports the following transfer modes:
        
- By line. Sends one line of the data logger per packet.
 - By variable. Sends one or more variables with their related information.
 
     TIP: 
    If the data logger mode is set to 
Value change
, the sampled values change only if one of the monitored variables changes.  Push Agent sends the values of a certain variable only if the variable value differs from the previously sent value.Provide Feedback