Alarm grid
    Use the 
Alarm grid
 widget to display and manage alarms at runtime. The Alarm grid
 widget allows you to display and manage the alarms at runtime. View alarm information and acknowledge and confirm the alarms.Each row in the grid indicates a change in alarm status. Acknowledge and confirm one or all alarms on the grid. The 
    
Alarm grid
 widget displays these columns of information:
      
  Column  | Description  | 
|---|---|
Timestamp  | Date and time of the last alarm event update.  | 
Name  | Name of the alarm object that generated the alarm event.  | 
Source variable  | Variable the event monitors.  | 
Message  | Message associated with the alarm event.  | 
Active  | Whether the alarm is:
                   Inactive  Active | 
Acknowledged  | Whether the alarm is acknowledged or unacknowledged:
                   Unacknowledged  Acknowledged | 
Confirmed  | Whether the alarm is confirmed or unconfirmed:
                  Unconfirmed  Confirmed | 
Severity  |  Level of alarm severity from 1 to 1000.   | 
The 
Alarm log grid
 widget displays alarm events recorded by the configured event logger, such as the Alarm History Grid
. Use the Alarm History Grid with filter
 widget to filter logged data.You can customize the data that appears in the 
Alarm grid
 by adding additional properties to an alarm to create an alarm type. See Create an Alarm grid.Provide Feedback
 Inactive
 Active
 Unacknowledged
 Acknowledged