Change the interface language
    Change the interface language to display a different language throughout the 
FactoryTalk Optix Studio
 application at design time and runtime. - To change the interface language, either:
- InProject view, select the project node and then inProperties, expandLocalizationand inLocales, select the language.
 - Selectand then in
 FactoryTalk Optix Studio OptionsLanguage and Locale, select the language. - Have a different user with a different associated locale language log on.
 
 
Provide Feedback